5 Electrical Safety Risks You Can Engineer Out Before They Reach The Field
Electrical safety outcomes are largely determined during design, not during installation or commissioning. For projects that rely on integrated electrical buildings, risk is influenced not only by the equipment selected, but by how that equipment is housed, arranged and delivered.
Below are five common risks and how they can be engineered out before systems reach the field.
Arc Flash Exposure
The Risk: Personnel are exposed to high-energy arc flash events during operation or maintenance.
Why It Happens: Switchgear and distribution equipment are installed without sufficient containment, isolation, or separation within the overall layout.
How to Engineer It Out: Integrate arc-resistant equipment within building designs that isolate energized components, incorporate defined working distances, and separate operational zones to limit exposure.
Excessive Field Installation Work
The Risk: Extended on-site installation increases exposure to hazards, schedule pressure, and variability in quality.
Why It Happens: Electrical equipment, building structures, and supporting systems are delivered separately and assembled in the field. This requires multiple trades working in the same space under tight schedules, increasing congestion, coordination complexity, and the likelihood of rushed or incomplete installation.
How to Engineer It Out: Use prefabricated, factory-integrated electrical buildings where switchgear, controls, and support systems are installed, wired, and tested before delivery, which reduces field labor and exposure time.
Cable Overcrowding and Heat Build-Up
The Risk: Congested cable routing increases heat, accelerates insulation degradation, and elevates fire risk.
Why It Happens: Electrical cables generate heat under load. As more cables are added into the same pathway or space, airflow is reduced and heat becomes trapped between conductors. This creates localized hot spots and requires derating, increasing the likelihood of insulation degradation and long-term failure.
How to Engineer It Out: Design electrical buildings and distribution systems to avoid dense cable routing. Maintain adequate spacing, defined pathways, and airflow to manage heat as systems scale, preserving both performance and safety within the enclosure.
Fire Risk and Fault Propagation
The Risk: Internal faults escalate into fires or spread across equipment, increasing damage and risk to personnel.
Why It Happens: Electrical equipment is not adequately compartmentalized or housed in structures designed to contain faults.
How to Engineer It Out: Incorporate fire-resistant construction, equipment separation, and compartmentalized layouts that contain faults and prevent propagation within the building.
Unsafe Maintenance Access
The Risk: Routine maintenance requires personnel to work in close proximity to energized equipment or in constrained spaces.
Why It Happens: Building layouts prioritize footprint or equipment density over safe access and serviceability.
How to Engineer It Out: Design buildings and equipment layouts with clear access zones, separation of energized compartments, and service-friendly configurations that reduce exposure during maintenance.
Designing Safety into the Building
Electrical safety is not only a function of the equipment but also a function of how that equipment is integrated, arranged, and delivered. Buildings that are engineered as complete systems, including enclosure, equipment, layout, and access, reduce variability and exposure across installation and operation.
For engineering, project, and procurement teams, this shifts the focus from managing risk in the field to reducing it through design decisions made upstream.