Skip to main content

Expandability

Expandability

Expandable nVent TRACHTE Buildings for Future Growth

nVent TRACHTE buildings are expandable at the end walls, which gives clients the ability to plan for convenient, fast, and economical future expansion. nVent TRACHTE’s built-in expandability can save clients’ money, both in the initial cost for a smaller building, and by lowering the continuous operating costs incurred heating, cooling, and ventilating an unnecessarily large building for the entire time the building is in service.

  • Existing buildings can be expanded by removing the end walls.​
  • Save initial construction and operating costs by purchasing a smaller building and adding on later.​
  • Add on to an existing building and keep the original end walls as a partition between two rooms.​
  • Previous end wall that become partitions can be re-finished with liner panel on both sides.​
  • Fire-Resistant Construction can be added to the previous exterior end wall such as for battery systems.​
  • We can add or remove doors as needed per the new configuration.​

 

Cable tray, wireway, and wiring can be preconfigured for easy electrical service connection to the existing building/section for fast and convenient building expansion.

Building Additions & Retrofits

nVent TRACHTE prefabricated buildings are designed and constructed with expandability and can be extended in the length dimension on either end wall. nVent TRACHTE’s Sales & Design Departments collaborate with clients to understand their building expansion needs and then design and produce a prefabricated, modular addition, specifically for their project.​

nVent TRACHTE’s Field Service Team will make the required modifications to the existing building and then install the new prefabricated expansion section in an efficient and seamless transition process requiring minimal on-site time and capital. 

Please contact nVent TRACHTE Sales with inquires regarding expanding an existing nVent TRACHTE building.

Untitled-2.gif

Get in Touch

Connect with one of our experts about your next project.