Skip to main content
Please Select Your Country and Language Preferences
Changing your location may affect product availability. Certain products may not be available in all international regions.
Current Selected Country: Algeria | English
Search for nVent products, resources, or ask any question you have
Loading search…

Discover the Difference with Liquid Cooling

Data Center Liquid Cooling Solutions

Efficient Liquid Cooling For High-Performance Computing

Liquid cooling solutions can provide significantly higher cooling efficiency compared to traditional air-cooling methods. Our hybrid liquid-to-air solutions help customers prepare data centers for next generation technology without completely rebuilding data center architecture.

Liquid Cooling at Scale for AI

Liquid cooling is vital for scaling AI as it effectively manages the heat produced by high-performance computing systems. This approach improves reliability, lowers energy usage, and accommodates the heavy computational requirements of AI tasks.
 

Stay cool under pressure – check our services! 


Industry Leaders Collaborate to Advance High Performance Computing

nVent is proud to collaborate with industry experts to develop innovative technical designs aimed at addressing the most challenging high-density compute cooling issues. With over 15 years of experience in liquid cooling, nVent’s deep technical application experience and global presence enables creating efficient solutions that ensure optimal performance and reliability for advanced computing environments for our partners.


Liquid Cooling Solutions for AI and HPC Workloads

02 DNS news thumb2

The Coolant Distribution Units(CDU) is the heart of the liquid cooling system, pumping the fluid at the desired temperature directly to the chips or servers.

02 DNS news thumb

The nVent Liquid-to-Air LTA Sidecar Heat Rejection Unit (HRU) is an integrated system that supports up to two racks of liquid-cooled IT equipment without a Facility Water System (FWS).

02 DNS news thumb3

Rear Door Heat Exchanger (RDHX) offer resilient operations with tool-less, hot-swappable components. The RDHX PRO upgrades data centers for high-density racks up to 78 kW, enhancing energy efficiency and space utilization.

Liquid Cooling FAQs
 

What is Liquid Cooling?

Liquid provides a much greater heat transfer capacity, 3,500 times higher than that of air, because liquid is denser than air. Liquid cooling can also dramatically increase the power usage effectiveness (PUE), reducing energy costs and contributing to environmental sustainability.

How Does Liquid Cooling Work?

There are three primary types of liquid cooling:   

  • Indirect liquid-cooled: heat is transferred to liquid through an air-to-water heat exchanger located within a row or cabinet.    
  • Direct liquid-cooled: heat is transferred directly to an attached liquid-cooled heat transfer component, such as a cold plate or immersion cooling.   
  • Hybrid direct and indirect water-cooled: selective cooling of the highest energy-consuming components with direct contact liquid cooling, with the balance of the cabinet cooled via a secondary air-to-water cooling device.  

Liquid Cooling vs Air Cooling in Data Centers

When air cooling systems need to work overtime to maintain necessary operating temperatures, facilities can experience equipment failures, unplanned downtime, and high energy costs. Air cooling is becoming less feasible in high-density data centers, as heat loads increase and server racks become so densely configured that air circulation is impeded. Liquid cooling systems, however, offer effective solutions for achieving required temperature parameters and lowering the energy consumption of the cooling system, thus lowering operating costs. Many new high-performance servers are designed with liquid cooling in mind.  


Liquid Cooling Insights

With all the expansion in AI, many new IT and chip technologies are being designed with liquid cooling in mind.

Data centers that only deploy air cooling may struggle to meet the demands of their customers in the future as they seek improved performance and next-generation IT equipment. 

TrendForce’s recent report states that the launch of NVIDIA’s Blackwell platform is set to drive the adoption of liquid cooling solutions from around 10% in 2024 to over 20% in 2025.  

Many data center managers and IT professionals are turning to liquid cooling. Liquid cooling can help data centers increase capacity while maintaining efficient space and energy use. These systems can provide an effective solution for achieving the required temperature parameters of next-gen chips and reducing the energy consumption of cooling systems. 

 RackChiller CDU800 Coolant Distribution Unit

liquid cooling page images_02 Why Liquid Cooling.webp

What Does it Take to Make the Switch to Liquid Cooling?

Constant advancements in technology and connectivity are driving new applications and an increased need to safeguard the world’s data and networks. Content streaming, online banking, cloud computing, edge computing, artificial intelligence. These are just a few examples of applications driving data demand around the world.  

As demand for internet and cloud services rises, data centers are being asked to exponentially scale capacity. In many cases they need to do this without dramatically increasing the physical space they occupy. Electrification is also driving next-generation technologies that outpace the ability of traditional data infrastructure—especially in the area of cooling. The time to consider liquid cooling is now.


Three Key Technologies for The Liquid Cooled Data Center

The acceleration of AI and high-performance computing is changing the landscape of the data center cooling industry. Next-generation technologies, including NVIDIA GPUs, require liquid cooling. This technology is here to stay and expanding every year; data center managers need to think about how, not if, they will bring liquid cooling capabilities into their data centers.  

Liquid cooling uses chilled water instead of air to capture and transport heat away from chips. It can offer better performance while saving energy and helping data centers operate more sustainably. 

Liquid provides a much greater heat transfer capacity than air, which helps increase power usage effectiveness (PUE), reducing energy costs and contributing to environmental sustainability.

liquid cooling page images_06 Explosive AI Growth.webp

Resources

DNS Cooling Brochure Mock-up.webp

Our comprehensive cooling solutions portfolio includes adaptable, modular and scalable solutions for networking, data center and communications applications.

We're here to help. 

Need more information? Contact us to learn more about our Networking, Data Center and Communications applications. One of our representatives will reach out to you shortly.

DNS contact.webp