Skip to main content
Please Select Your Country and Language Preferences
Changing your location may affect product availability. Certain products may not be available in all international regions.
Current Selected Country: Jordan | English
Search for nVent products, resources, or ask any question you have
Loading search…

Service Request for Cooling Units

Service Request for Cooling Units

Step 1. Troubleshooting guide to find a solution for your issue:

1. Excessive formation of condensate

Cabinet with degree of protection less than IP54

a. Check that the self-adhesive rubber seal between the air conditioner and the cabinet has been applied properly

b. Check that the closing panels of the condenser have been properly assembled

c. Check that there are no openings in the cabinet

2. Does not cool adequately

Internal fan runs, compressor and external fan operate intermittently

a. Clean the evaporator

b. Make sure that there are no external causes which limit the flow of air inside circuit

Condenser fan and evaporator fan operate and compressor operates intermittently

a. High pressure switch intervention, when present
 

Ambient temperature higher than the maximum allowed by the rating plate

  • Ventilate the room

Please fill in the detailed error description and send the form

  • Dirty filter

Clean or if necessary replace the dirty filter

  • Dirty exchange condenser

Clean the condenser

  • Ventilation short-circuiting

Make sure that no obstructions or obstacles may cause exhaust air short-circuiting

Check that the minimum distances from a wall, ceiling, electrical cabinet or another air conditioner is respected as indicated in this manual

 

b. Compressor thermal protector intervention

Air temperature in the cabinet higher than the maximum value allowed by the rating plate of the unit

 

Same causes and remedies reported at 2.a

Internal fan operates, external fan does not operate, compressor operates intermittently

a. Faulty fan electric condenser

  • Replace the electric condenser

b. Faulty external fan

  • Replace the condenser fan

3. Does not cool

None of the components operate

a. No voltage to the unit

  • Make sure doors and switches are closed
Compressor, condenser fan and evaporator fan operate

a. Insufficient gas charge in the cooling system

  • Please fill in the detailed error description and send the form

b. Compressor mechanical fault

  • Please fill in the detailed error description and send the form
External fan and internal fan operate, compressor does not operate

a. Faulty fan electric condenser

  • Replace the electric condenser fan

b. Faulty evaporator fan

  • Replace the fan
External fan, internal fan and compressor operate

a. Adjusting thermostat faulty or set at a temperature higher than the temperature in the cabinet

4. ALARM

ALARM

P1, P4, HA, LA, HP, SEC, HAS,

Please fill in the detailed error description and send the form.

Step 2. Service Request for Cooling Units

If the issue with your air conditioner persists after trying the troubleshooting steps, please complete the form below. Have your Air conditioner details at hand, as you will need to provide them to submit the form. Refer to the image below for your product information.